Technical FAQs

Ask a Question

What is the part number of the power supply used with the 8030ICM200?

The 8030ICM200 does include a power "Y" cable to power the unit off of a PCs keyboard port. The unit may also be powered from an external power supply. While Schneider Automation does not offer a power supply for the 8030ICM200, a power supply can be purchased from any vendor having the following specs:
minimum 200 mA
Regulated 5 Volts (+/-10%)
Switchcraft S760 connector with +5V on inside conductor


Legacy KB System (APS) Data: RESL164416 V1.0, Originally authored by on , Last Edited by on
Related ranges: Sy/Max
Was this helpful?
What can we do to improve the information ?