Technical FAQs

Ask a Question

Is there a way to get the ProWORX NxT software to come up in PROGRAM mode when you go directly on-line to the controller?

Yes, there is a way to get ProWORX NxT to come up in PROGRAM mode when going on-line to the controller. In the NxT Preferences, for the On-line Mode option, select "Program". The default Preference setting is Monitor mode.

 
Was this helpful?
What can we do to improve the information ?