Technical FAQs

Ask a Question

Why is the 'Optimize Project' option grayed out in Concept?

In order to optimize a project the project must be closed. Once the project is closed, choose File>>Optimize Project and navigate to the location of the project on your computer.
NOTE: Optimizing a project will cause Concept and the PLC to become 'Not Equal' and will require that you stop the PLC and perform a full download.

Was this helpful?
What can we do to improve the information ?