Technical FAQs

Ask a Question

What does the value of a thermocouple read, when a broken wire occurs on the Compact ADU257?

The value would read the minimum scale of the temperature range if configured to read actual temperature or 0 if configured to read counts.


Legacy KB System (APS) Data: RESL164164 V1.0, Originally authored by on , Last Edited by on
Related ranges: Compact
Was this helpful?
What can we do to improve the information ?