Technical FAQs

Ask a Question

Can I use 115VAC inputs with Twido?

Yes, to do so it is necessary to use the new 115 VAC input expansion module TWDDAI8DT.


Legacy KB System (APS) Data: RESL164091 V1.0, Originally authored by on , Last Edited by on
Related ranges: Twido
Was this helpful?
What can we do to improve the information ?