Technical FAQs

Ask a Question

What is the Concept Application Loader?


The Concept Application Loader (372 SPU 477 01 V26. ) is a simple tool to download Concept 2.6 Projects. It is a stripped down version of Concept with no on-line editing capability, no saving of an application, no changes to the configuration, and no viewing of the application code. The Reference Data Editor will be available. For projects that are protected the reference data editor will be available in read only mode.


Legacy KB System (APS) Data: RESL163987 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?