Technical FAQs

Ask a Question

Which PLC product line is associated with the TSXSUP1051 power supply?

The TSXSUP1051 power supply doesn't belong to any one particular PLC product line. It's an external 24v power supply that can be used with any PLC product line. The power supply will not mount to any backplane but can be mounted onto a Din rail.


Legacy KB System (APS) Data: RESL163867 V1.0, Originally authored by on , Last Edited by on
Related ranges: Other PLCs
Was this helpful?
What can we do to improve the information ?