Technical FAQs

Ask a Question

What are the power requirements for my fiber optic repeater?

The power requirements are determined by the model used. The models are powered as seen below:
.
The power requirements are determined by the type and range of power applied:
.


Legacy KB System (APS) Data: RESL163865 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modbus Plus
Was this helpful?
What can we do to improve the information ?