Technical FAQs

Ask a Question

What would cause a 'General Protection Fault in the GLFS31BW.dll' in Concept 2.6 SR1 when running Windows XP Pro?

This error is often generated because of the display settings for the PC. Settings of 1400 x 1050 or 1024 x 768, depending on the PC, are recommended.


Legacy KB System (APS) Data: RESL163677 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?