Technical FAQs

Ask a Question

Can I use a PCMCIA card that is larger than 16Mb with my XBTF Magelis screen?

Yes, a larger card may be used. Schneider does not sell a larger card for use with the Magelis, but a Type II PCMCIA flash card may be used.


Legacy KB System (APS) Data: RESL163597 V1.0, Originally authored by on , Last Edited by on
Related ranges: Magelis XBT-F, TXBT-F
Was this helpful?
What can we do to improve the information ?