Technical FAQs

Ask a Question

What would cause a Quantum 140CPS11100 power supply to not power up?

The Quantum 140CPS11100 power supply that has a PV 01 or higher now require a jumper on pins 3 and 4 on the terminal strip for 115 VAC operations. If this jumper is not installed, it will be set for 220 VAC operations. Any power supply with a PV less than 1 did not require the jumpers.


Legacy KB System (APS) Data: RESL163548 V3.0, Originally authored by DiSa on 08/17/2007, Last Edited by DiSa on 08/17/2007
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?