Technical FAQs

Ask a Question

Can the Sy/Max PS25 and PS35 power supplies be mounted outside the rack?

Yes, the 8030PS25 and 8030PS35 power supplies can be mounted outside the rack. This will require the 8030ADP100 mounting bracket and the 8030CC15 power cable. The 8030PS35 comes with the cable and bracket, but these items must be ordered separately for use with the 8030PS25.


Legacy KB System (APS) Data: RESL163521 V1.0, Originally authored by on , Last Edited by on
Related ranges: Sy/Max
Was this helpful?
What can we do to improve the information ?