Technical FAQs

Ask a Question

What is the maximum length of a Fipway optical network segment?

The maximum network length of a Fipway optical segment (between two TSXFPACC8 optical repeaters) is 3000 meters.

Was this helpful?
What can we do to improve the information ?