Technical FAQs

Ask a Question

Is there an Advantys keying pin kit available for I/O to base connection?

Yes there is a kit available. If you want to key the I/O module to a base connection, use the module keying pin kit part number STBXMP7700. This kit contains a quantity of 60.

 
Was this helpful?
What can we do to improve the information ?