Technical FAQs

Ask a Question

174CEV30010 Modbus to Ethernet Bridge Upgrade - V1.8

Goals and Symptoms

To inform of readers of the changes incorporated into the exec V1.8 for the CEV bridge.
To Inform readers how to upgrade an existing 174CEV30010 bridge to V1.8

Facts and Changes

The following changes are made in the V1.8 version of the 174CEV30010 Exec:
Improved Support for the TCP connection management
All Schneider 174CEV30010 units can be upgraded to V1.8

Causes and Fixes

New firmware can be loaded into the 174CEV30010 bridge using a TFTP client.
Please note that TFTP is not as reliable as FTP and several attempts may be required to successfully load new firmware into the bridge.
The steps required are :
Obtain a TFTP client program.
These are available from many sources, for example Walusoft offers a TFTP see, http://www.walusoft.co.uk/download.htm

Extract the supplied ROM file to your PC.

Start the TFTP transfer utility and transfer the ROM file to the 174CEV30010.
If upgrading an pre V1.6 bridge the destination file name is 4D. or ZD
Once V1.6 is installed the destination file name will be CV.

Example Upgrade using Walusoft TFTP Client:


Check that the new Firmware is installed:
Connect to the bridge setup screens, the introduction screen should now show V1.8

Attachments

(Removed File URL: 163376_5842/CV0180.ROM)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/142825376c8c06dc85256f000058193d/fl_block_5/0.1398?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL163376 V2.0, Originally authored by on , Last Edited by on
Related ranges: ConneXium - Ethernet
Was this helpful?
What can we do to improve the information ?