Technical FAQs

Ask a Question

What does 'NaN' mean when displayed in the Concept RDE or as an animated value in the logic editor?

'NaN' means 'not a number'. At this point troubleshooting is necessary to determine where this value is coming from.


Legacy KB System (APS) Data: RESL163343 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?