Technical FAQs

Ask a Question

Is state ram included when exporting a Concept project using the Concept Converter?

Yes, the contents of state ram (4X register contents) and discrete input and output disabled states are included in the export and are visible through the reference data editor after the project has been imported.


Legacy KB System (APS) Data: RESL163267 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?