Technical FAQs

Ask a Question

What is the function of the "Rebuild Database" feature in the ProWORX NxT software?

The "Rebuild Database" function reconstructs the database descriptor file (.DPF) from the existing (.DDF) file. This may be necessary if the (.DPF) file is ever corrupted or accidentally erased.


Legacy KB System (APS) Data: RESL163218 V2.0, Originally authored by PeZa on 09/11/2010, Last Edited by RoAl on 09/11/2010
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?