Technical FAQs

Ask a Question

What are the part numbers for the various Quantum backplanes?

Here is a list of the various Quantum backplanes:

text
Part Number
text
Number of Slots
text
Length
text
140XBP00200
text
2
text
4 inches
text
140XBP00300
text
3
text
5.6 inches
text
140XBP00400
text
4
text
7.2 inches
text
140XBP00600
text
6
text
10.4 inches
text
140XBP01000
text
10
text
16.7 inches
text
140XBP01600
text
16
text
26.4 inches

Legacy KB System (APS) Data: RESL163216 V2.0, Originally authored by PeZa on 06/18/2010, Last Edited by RoAl on 06/18/2010
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?