Technical FAQs

Ask a Question

Is a DeviceNet connector included with the Momentum DeviceNet communication adapter 170LNT71000?

No, the DeviceNet connector is not included with the communication adapter and can be ordered separately. The connector part number is 170XTS06000.


Legacy KB System (APS) Data: RESL163198 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Momentum
Was this helpful?
What can we do to improve the information ?