Technical FAQs

Ask a Question

How can I print my Concept project to a 'file'?

Printing to a FILE: in Concept:

To print to a file in Concept, go to <Start><settings><printers> and 'Add a printer'. Make it a local printer and choose the following port:
FILE: (Print to File). Choose 'Generic' as the manufacturer and 'Generic/Text Only' as the Printer.

It will now be a choice in the Concept 'Printer setup'. Choose it as your printer and set up your print options.


Legacy KB System (APS) Data: RESL163096 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?