Technical FAQs

Ask a Question

Is the AS-E908-031 S908 executive cartridge compatible with the PC-E984-X8X controllers?

No. The AS-E908-031 executive cartridge are not compatible with the PC-E984-X8X at any prom combo. If a user is migrating from a PC-0984-X8X controller to a PC-E984-X8X controller and if the executive cartridge in the S908 Remote I/O module is a AS-E908-031, then the user must purchase a new executive cartridge. The current part number is AS-E908-131. Its current prom combo is 1011. The minimum prom combo required for the AS-E908-131 executive cartridge to be compatible with the PC-E984-X8X controller is 1007.


Legacy KB System (APS) Data: RESL163007 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon 1/2/3/4/5/8/984s
Was this helpful?
What can we do to improve the information ?