Technical FAQs

Ask a Question

What is the maximum length for an AS-i bus network?

The maximum length is 100 meters, this includes the cabling for the main run as well as the branches connecting the AS-i slaves.


Legacy KB System (APS) Data: RESL162973 V1.0, Originally authored by on , Last Edited by on
Related ranges: AS-Interface
Was this helpful?
What can we do to improve the information ?