Technical FAQs

Ask a Question

Can you increase the available current on a DIO drop by adding an additional power supply?

Yes, one can increase the 3A of available bus current provided by the 140CRA21x10 drop module.
In applications where the DIO Adapter's internal power supply ( rated at 3A) does not have enough power for the number of modules or the amount of power required, users can install a Quantum Standalone or Summable power supply to allow for up to 11A of bus current.
To use this configuration the user must render the internal supply for the DIO Adapter unpowered by removing the connection to the module's input. Also, the added power supply must NOT be added to the system I/O Map.

Please refer to the Modicon Quantum Automation Series Hardware Reference Guide (840USE10000 v 10.0) for listing of compatible power supplies and technical details.

Legacy KB System (APS) Data: RESL162852 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?