Technical FAQs

Ask a Question

In ATV28, We can write "8002H" to CMD to run Motor( normal ), write "8802H" to CMD to run Motor( reverse ), and write "9002H" to CMD to STOP Motor, H...

Goals and Symptoms

In ATV28, We can write "8002H" to CMD to run Motor( normal ), write "8802H" to CMD to run Motor( reverse ), and write "9002H" to CMD to STOP Motor, How to maintenance ATV31 by this way?

Facts and Changes

CMD

Causes and Fixes

On the ATV31 there is no problem if the bit 15 is not use for a special function ( menu FUN ) if not, you need to follow the Drivecom bause there will a conflict between the both functions of bit 15.


Legacy KB System (APS) Data: RESL162789 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 31
Was this helpful?
What can we do to improve the information ?