Technical FAQs

Ask a Question

What is the difference between the AS-B804-016 and the AS-B804-116?

The part number change reflects component and board layout changes necessitated by a vendor change. These changes do not affect customer functionality, there are no changes to the electrical specifications, and this version is directly slot-replaceable with existing B804. The B804-116 used led's as opposed to neon's and LED's would be logic side indicators rather than field side indicators.


Legacy KB System (APS) Data: RESL162772 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon 1/2/3/4/5/8/984s
Was this helpful?
What can we do to improve the information ?