Technical FAQs

Ask a Question

FAULT ILF IN ALTIVAR 58. WHEN REPETITIVE UDP FRAME OF 1525 BYTES (POLLING RATE 5 MS) IN NET.

Goals and Symptoms

FAULT ILF IN ALTIVAR 58. WHEN REPETITIVE UDP FRAME OF 1525 BYTES (POLLING RATE 5 MS) IN NET.

Facts and Changes

16 UNITS OF VW3A58310. WHEN REPETITIVE UDP FRAME OF 1525 BYTES POLLING RATE 5 MS

Causes and Fixes

Be careful, with UDP there is no guarantee on the datagram validity , if the datagram in not complete the inverter will trip in ILF, and it's necessary to have some time to analyse 1525 bytes and a clogging is possible at the input card, try to increase the polling and if it's possible use the TCP mode.

USER MANUEL P100 English version : The Ethernet card is compliant with ETHERNET 2 frames format (IEEE 802.3 is not supported).

If you server can support only this mode, the only solution is to replace it.


Legacy KB System (APS) Data: RESL162681 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 58
Was this helpful?
What can we do to improve the information ?