Technical FAQs

Ask a Question

How can I customize the ProWORX NxT network display screen?

Open the NxT network display screen by selecting 'VIEW' then 'NETWORK DISPLAY SETUP'. Select the "Custom Screen Setup" option to create your own view format. You can display up to seven lines of information for each logic element, five lines above the instruction and two lines below it. You have six options to choose from:
Addr: the instructions' address.
Desc1 to Desc9: descriptor lines 1 to 9.
Symb1 to Symb2: symbol lines 1 to 2.
BRef: back-referencing information.
Data: the value stored at the address.
Clear or Blank: leaves the display line blank.

Was this helpful?
What can we do to improve the information ?