Technical FAQs

Ask a Question

Comment alimenter un XBTN200/400 pour transférer une application de XBTL1000. How to energize a XBTN200/400 to transfer an application from XBTL1...

Goals and Symptoms

Comment alimenter un XBTN200/400 pour transférer une
application de XBTL1000.

How to energize a XBTN200/400 to transfer an application from
XBTL1000.

Facts and Changes

XBTN

Causes and Fixes

See attachement

Attachments

(Removed File URL: 162612_5596/Connection_XBTN_PC.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/a9db8504accca16d85256e99004ee44b/fl_block_5/0.13BC?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL162612 V1.0, Originally authored by on , Last Edited by on
Related ranges: Magelis XBT-N
Was this helpful?
What can we do to improve the information ?