Technical FAQs

Ask a Question

Do you know the color code of ATV38? (In China, we use a serial number to define different color ,that is color code,for instance Red is GB-0001 etc....

Goals and Symptoms

Do you know the color code of ATV38? (In China, we use a serial number to define different color ,that is color code,for instance Red is GB-0001 etc. It is a color standard.I am not sure if it is the same in France?)

Causes and Fixes

The color of plastic is RAL7030, it's a standard in Europe and it's possible to have more details with a painting manufacturer.

Was this helpful?
What can we do to improve the information ?