Technical FAQs

Ask a Question

Why do I get a "PROM NOT ERASE" error on my 8005PR4 when I try to burn a new program to a 8005MP14?

The 8005PR4 can only burn programs to a blank 8005MP14. The user must use a UV Prom eraser in order to erase a 8005MP14. The MP-14 is a EPROM cartridge, not a EEPROM cartridge.


Legacy KB System (APS) Data: RESL162570 V1.0, Originally authored by on , Last Edited by on
Related ranges: Sy/Max
Was this helpful?
What can we do to improve the information ?