Technical FAQs

Ask a Question

How do I read/ write a program to/ from a 8005MP24 from/ to a 8005PR4 hand held programmer?

To read the program out of a mem pack into the PR-4's memory use the following key sequence: PROM+ READ + ENTER.
To burn 8005MP24 EEPROM with a program from the 8005PR4 use the following key sequence: PROM + ENTER + ENTER.


Legacy KB System (APS) Data: RESL162567 V1.0, Originally authored by on , Last Edited by on
Related ranges: Sy/Max
Was this helpful?
What can we do to improve the information ?