Technical FAQs

Ask a Question

How do I "jump" over a group of rungs in Unity Pro - LD logic?

When a Unity Pro LD section is opened two icons are displayed on the menu bar that are used to skip logic.
The ' ->>' jump icon is used at the beginning of the logic you want to skip and the skip ends with a 'JL:' .

The '->>' link must reference the JL: label. For example, the General comment for the '->>' would be 'JumpOut'.
and the General comment for the 'JL:' would also be 'JumpOut'. The General comment is limited to 32 characters
and must be unique across the entire section.
The 'JL:" must come off the left power rail.
 


Legacy KB System (APS) Data: RESL162473 V1.0, Originally authored by on , Last Edited by on
Related ranges: Unity Pro
Was this helpful?
What can we do to improve the information ?