Technical FAQs

Ask a Question

Why do I get error message "There is not enough room on disk drive C:\884FolderName to create the BIN file" when creating a new database in the ProWorx 884 software?

To eliminate the "There is not enough room on disk drive C:\884FolderName to create the BIN file" error, you have two options when creating a new ProWorx 884 database:
1) Create a new 10Meg partition on your hard-drive other than the C: drive. This is because the ProWorx 884 DOS software was created a long time ago when hard-drives were no bigger than 20Meg. Anything over 20Meg and the ProWorx 884 software will see it as not enough disk space.

2) Create a new ProWorx 884 database and put it into the A: floppy drive. Then copy the new ProWorx 884 database files from the A: floppy drive and place them into your C:\884FolderName folder. You can then go into the C:\884FolderName folder, select and open the database and start programming.


Legacy KB System (APS) Data: RESL162427 V1.0, Originally authored by on , Last Edited by on
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?