Technical FAQs

Ask a Question

What is the maximum number of registers the SyMax Model 400 processors can use for addressing?

The SyMax Model 400 processor, which includes model types SCP401, 423, 424 and 444, contains 4000 on-board registers. This is the maximum number it is capable of addressing.


Legacy KB System (APS) Data: RESL162424 V2.0, Originally authored by PeZa on 12/14/2010, Last Edited by RoAl on 12/14/2010
Related ranges: Sy/Max
Was this helpful?
What can we do to improve the information ?