Technical FAQs

Ask a Question

ATV16-ATV28 In case of ATV16's SLP parameter is ON , which value should I apply to ATV28's SLP parameter? On is toward 5 or 0?

Goals and Symptoms

ATV16-ATV28 In case of ATV16's SLP parameter is ON , which value should I apply to ATV28's SLP parameter? On is toward 5 or 0?

Causes and Fixes

If you use the factory setting value, it will similar to the ATV16 value with an average of +/- 0,5 Hz.
It's also available for the ATV18.

To be clear, on the ATV16 the SLP value was fixed at 5 Hz ( not possible to adjust it ) but you can adjust the SLP from 0 to 5 Hz on the ATV28 ( fault value is 5 Hz )


Legacy KB System (APS) Data: RESL162356 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 28
Was this helpful?
What can we do to improve the information ?