Technical FAQs

Ask a Question

How can I change the Event Log file path in Concept 2.6?

The log file path can only be changed when all projects are closed. When a project is opened after the path has been changed, the change is reflected in <Options><Preferences><Common> and is greyed out.

Was this helpful?
What can we do to improve the information ?