Technical FAQs

Ask a Question

ATV 31 modbus comms with LUFP1.I need application examples and short cuts and configuration for the drive.

Goals and Symptoms

ATV 31 modbus comms with LUFP1.I need application examples & short cuts & configuration for the drive.

Facts and Changes

ATV 31 with LUFP1 to premium plc

Causes and Fixes

There is nothing for the drive, only the baudrate and address, example in attachments.

Attachments

(Removed File URL: 162238_542E/Appli_ATV.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/870f29ca3457766285256ea90047269b/fl_block_5/0.612?OpenElement&FieldElemFormat=gif)(Removed File URL: 162238_542E/App_LUFP1_ATV.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/870f29ca3457766285256ea90047269b/fl_block_5/0.113C?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL162238 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 31
Was this helpful?
What can we do to improve the information ?