Technical FAQs

Ask a Question

Hi, We did promotion on the ATV58 with the ethernet optionmodule (V2). We are using the rollname (DHCP) service and FDR . This is working fine , but o...

Goals and Symptoms

Hi, We did promotion on the ATV58 with the ethernet optionmodule (V2). We are using the rollname (DHCP) service and FDR . This is working fine , but on one condition these features are not working. When the ATV is powered off , and the switch or hub to whom he is connected aswell. Power on the Altivar first and after a minute the switch or hub, then the altivar will not obtain his IP adres. We have a similar situation with the STB modules . This is urgent.

Facts and Changes

ATV58 Ethernet

Causes and Fixes

Running of DHCP and FDR :

After power on, the option card send the DHCP requests during a time of 64 sec, so if you power on the switch or hub after 1 min ( 60 sec ) there is not enough time to receive the DHCP answer and the card is lock, you can verify this with the embedded server and the FDR status.


Legacy KB System (APS) Data: RESL162219 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 58
Was this helpful?
What can we do to improve the information ?