Technical FAQs

Ask a Question

How many copper FIPIO or FIPWAY network segments can be joined into one copper FIP network and what is the total length possible?

Up to 5 copper FIPIO or FIPWAY network segments can be joined using either TSXFPACC6 (electrical) or TSXFPACC8 (optical) repeaters to get a total length of 5000m of copper cabling. Each individual segment is limited to 1000 meters in length. This figure includes all trunk cabling and all drop cabling.

Was this helpful?
What can we do to improve the information ?