Technical FAQs

Ask a Question

Do I need to terminate each FIPIO or FIPWAY network segment separately, or do I just need to terminate the end segments of the network?

Each FIP segment in the network needs to be terminated with the TSXFPACC7 line terminator at each end of the segment.


Legacy KB System (APS) Data: RESL162020 V1.0, Originally authored by on , Last Edited by on
Related ranges: Fipway - Fipio
Was this helpful?
What can we do to improve the information ?