Technical FAQs

Ask a Question

How many devices can be connected to a FIPIO or FIPWAY network?

32 nodes may be connected to a FIP network without a repeater. Usage of either TSXFPACC6 (electrical) or TSXFPACC8 (optical) repeaters allows up to 64 nodes to be connected to the FIP network.

 
Was this helpful?
What can we do to improve the information ?