Technical FAQs

Ask a Question

What are the valid addresses on a FIPIO or FIPWAY network and are there any addressing considerations?

Valid addresses on a FIP network are from 0 to 63. Address 0 is reserved for the PLC bus arbiter. Address 63 is reserved for a programming terminal. All nodes on the network must have a unique address.

Was this helpful?
What can we do to improve the information ?