Technical FAQs

Ask a Question

In the ProWORX NxT Traffic Cop print options, what's the difference between the Full, Brief and Visual printouts?

Full Option prints the entire Traffic Cop information and any attached documentation.
Brief Option prints a Traffic Cop overview and a summary of the documentation.
Visual Option prints a graphical representation of the brief option.


Legacy KB System (APS) Data: RESL161944 V3.0, Originally authored by PeZa on 12/14/2010, Last Edited by RoAl on 08/30/2013
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?