Technical FAQs

Ask a Question

What minimum voltage is it possible to use ATV68, when switching-off protection “undervoltage”?

Goals and Symptoms

What minimum voltage is it possible to use ATV68, when switching-off protection undervoltage? Thank you very much for your help.

Facts and Changes

ATV68,

Causes and Fixes

400 V range = 287 V
500 V range = 346 V
690 V range = 537 V

If the control is supplied with an external source 24V, if the voltage goes under the guarantied range, and if the fault undervoltage is deactivated (E3.08), the drive is going to supply the motor in downgraded operation (speed reduction, current limitation...) as long as no other fault appears.


Legacy KB System (APS) Data: RESL161862 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 68
Was this helpful?
What can we do to improve the information ?