Technical FAQs

Ask a Question

What is the power dissipation for the Quantum Low End CPU modules?

The following is a list of the power dissipation for all of the Quantum Low End CPU modules:

text
Quantum controller
text
Power Dissipation
text
140CPU11302
text
3.9 W
text
140CPU11303
text
3.95 W
text
140CPU21304
text
4.5 W
text
140CPU42402
text
9 W
text
140CPU43412
text
9 W
text
140CPU43412A
text
6.25 W
text
140CPU53414
text
9 W
text
140CPU53414A
text
6.25 W

Legacy KB System (APS) Data: RESL161609 V3.0, Originally authored by PeZa on 07/29/2010, Last Edited by RoAl on 07/24/2013
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?