Technical FAQs

Ask a Question

Using an ATV31 in Can_open bus. I' m using Sycon configurator software to configure my Can_open bus. Inserting the EDS file related to the ATV31 and t...

Goals and Symptoms

Using an ATV31 in Can_open bus. I' m using Sycon configurator software to configure my Can_open bus. Inserting the EDS file related to the ATV31 and trying to modify the EVENT TIMER parameter (Index 1805 Sub_index 05) from the Object Configuration window a message advise me that this operation can be performed using the Node Configuration window . Can someone explain me in which way ? I' m not able to find how to modify this parameter from Sycon.

Facts and Changes

ATV31 Can_open Sycon Configurator software

Causes and Fixes

In fact it's a bg of Sycon, it's not possible to modify the EVENT TIMER with it. ( Transmitted to the HUB activity ).


Legacy KB System (APS) Data: RESL161591 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 31
Was this helpful?
What can we do to improve the information ?