Technical FAQs

Ask a Question

What will cause an '-2222 - Internal error in file tiaifunc.cpp' error in Concept?

Error -2222 in Concept is caused by a corrupted DFB. Usually an ST section did not compile properly.
Export the project 'with used DFBs' and re-import.

Was this helpful?
What can we do to improve the information ?