Technical FAQs

Ask a Question

What causes a '-943 Failed to get address of priority description' error when opening a project in Concept?

This error occurs when opening a project if Concept had previously crashed while editing a project.
Close Concept and delete the Vista.log and Vista.taf files. Launch Concept and try to reopen the project.


Legacy KB System (APS) Data: RESL161499 V2.0, Originally authored by DaSo on 04/08/2011, Last Edited by DaSo on 04/08/2011
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?