Technical FAQs

Ask a Question

Which program should be used to configure Modbus parameters on gateway LA9P307? Where can I get this program?

Goals and Symptoms

Which program should be used to configure Modbus parameters on gateway LA9P307? Where can I get this program?

Facts and Changes

LA9P307 Modbus

Causes and Fixes

The program is ABC Configurator and you can find it inside the PowerSuite 2.0 CDROM ( VW3A8104 ).

Was this helpful?
What can we do to improve the information ?